Caterpillar Introduces 2,750 kW Diesel Generator Set with Industry-Leading Power Density for Standby Applications

For Worldwide Release: September 20, 2017
Release Number: EEPR1317

PEORIA, ILL. – Caterpillar Inc. today announced the introduction of the Cat® 3516E diesel generator set with a new 2,750 kW rating for 60 Hz standby applications. Certified to U.S. EPA Stationary Emergency Regulations, this reliable package features industry-leading power density to reduce total site preparation, transportation and installation costs while requiring less overall space for the generator set.  

The newly rated Cat 3516E generator set offers reliable backup power from a footprint of 220.8 square feet, saving up to 12 percent of installed space when compared with competing generator sets at similar ratings. It is the result of the on-going refinement of the Cat 3500 Series engine, which has demonstrated its performance and durability in hundreds of thousands of installations worldwide. 

The Cat 3516E high power-density generator set delivers the latest in a series of new ratings for medium- to large-sized diesel generator sets from 1,250 kW to 2,800 kW. These new ratings significantly reduce customers’ installed and ancillary costs through reduced overall footprints and weight. 

“The introduction of this uprated generator set adds to Caterpillar’s industry-leading portfolio of power solutions finely tuned to customer needs,” said Jason Kaiser, product manager for Caterpillar’s Large Electric Power Division. “It reflects how we are leveraging Caterpillar’s proven technology and deep knowledge of the market to continuously improve our customers’ return on investment.” 

The Cat 3516E generator set is designed to meet the NFPA power restoration requirement for Level 1 systems and accepts 100 percent block load in one step. It also meets ISO 8528-5 G3 requirements for steady state and load acceptance. 

This generator set can be equipped with a low- or high-voltage alternator. Both alternator options enable quick load acceptance and feature exceptional motor starting capabilities, allowing users to minimize oversizing the generator set due to motor starting requirements. 

The Cat 3516E generator set utilizes the field-proven Cat ADEM™ A5 engine control module (ECM), which integrates all engine functions including ignition, governing, air-fuel ratio control, and engine protection. 

Caterpillar is a leader in the power generation marketplace with power systems engineered to deliver unmatched durability, reliability and value. The company offers worldwide product support, with parts and service available globally through the Cat authorized service and dealer network. In addition, dealer service technicians are trained to service the entire Cat generator set and ancillary equipment. 

For more information, visit www.cat.com/powergeneration or e-mail cat_power@cat.com. To interact with other power generation professionals in our online community, register at http://forums.cat.com/powerperspectives

 

Available Images

Download here or contact Bob Chase at bchase@gelia.com

Cat® 3516E diesel generator set

# # #

About Caterpillar

For more than 90 years, Caterpillar Inc. has been making sustainable progress possible and driving positive change on every continent. Customers turn to Caterpillar to help them develop infrastructure, energy and natural resource assets. With 2016 sales and revenues of $38.537 billion, Caterpillar is the world’s leading manufacturer of construction and mining equipment, diesel and natural gas engines, industrial gas turbines and diesel-electric locomotives. The company principally operates through its three product segments - Construction Industries, Resource Industries and Energy & Transportation - and also provides financing and related services through its Financial Products segment. For more information, visit caterpillar.com. To connect with us on social media, visit caterpillar.com/social-media.

CAT, CATERPILLAR, BUILT FOR IT, their respective logos, “Caterpillar Yellow,” the “Power Edge” trade dress as well as corporate and product identity used herein, are trademarks of Caterpillar and may not be used without permission.

©2017 Caterpillar
All Rights Reserved

 

Press Inquiries

Bob Chase 
Gelia
Tel: +1 716-629-3230
bchase@gelia.com

Chuck Boysen
Caterpillar Inc.
Tel: +1 309-578-4962
Boysen_Charles@cat.com

 

Reader Requests Caterpillar Inc.
Electric Power Division
P.O. Box 0610
Mossville, IL 61552-0610